Polylactic acid (PLA): Supporting lactic acid fermentation yield
Effective PLA process control maximizes lactic acid fermentation yield by minimizing variability and protecting polymer quality.
Tóm lại
- Growing regulatory and environmental pressure on conventional plastics is driving adoption of PLA as a scalable bio‑based alternative.
- Scaling PLA production requires optimizing lactic acid fermentation yield while maintaining strict control of purity and stereochemistry.
- A measurement‑driven control strategy enables predictable, high‑yield industrial PLA production at scale.
Scaling polylactic acid (PLA) production for sustainable plastics
Polylactic acid in today's bioplastics landscape
Modern plastics have enabled major advances in safety, efficiency and product performance across nearly every industry. However, their durability, resistance to degradation and low production cost have also contributed to significant environmental pressures. Plastic pollution has emerged as a worldwide concern, with annual global production and waste doubling in 2019 compared to 2000.
Today, around 400 million tons of plastic are produced each year and this volume is forecast to triple by 2060. Only 9% of all plastic ever produced has been recycled, while the remainder has been burned, landfilled or released into the environment.
Marine ecosystems are particularly impacted, as mismanaged plastic waste quickly finds its way into rivers, coastlines and open oceans. Approximately 11 million tonnes of plastic enters the ocean every year. That's the equivalent of us dumping 2,000 garbage trucks full of plastic into the world's oceans, rivers and lakes every single day (UNEP, 2025). Projections warn that there could be more plastic by weight than fish in the sea by 2050.
Dữ kiện chính
~11 million of plastic
enters the ocean each year
Equivalent to 2,000 garbage trucks of plastic dumped every day
PLA: properties, production and applications
In response, the biobased polymers such as polylactic acid (PLA) provide a credible and scalable alternative for more sustainable material systems. PLA is a bio-based biodegradable polymer produced from lactic acid obtained through fermentation of starch-rich or sugar-rich feedstocks. These materials offer mechanical strength, transparency and processing versatility. It is widely used in packaging, textiles, consumer goods and 3D printing applications, including PLA filaments. As industries replace petroleum-derived plastics with renewable alternatives, PLA has become one of the most strategically important biopolymers in today's global sustainability landscape.
Worldwide regulations & adoption initiatives for PLA
According to the European Bioplastics 2025 Market Data Report , global biobased plastics production capacity is expected to increase from 2.31 million tonnes in 2025 to 4.69 million tonnes by 2030, driven by rising demand and ongoing material innovations. Bio-based plastics currently account for 0.5% of the 431 million tonnes of plastics produced globally each year.
In the European Union, the European Commission has issued EU policy framework on bio-based, biodegradable and compostable plastics, defining requirements for sourcing, labelling and application across sectors such as packaging, consumer goods and textiles.
In the United States, federal initiatives such as the USDA BioPreferred Program and EPA Sustainable Materials Management support the adoption and responsible use of bio‑based materials including PLA. Similarly in Japan, the Ministry of the Environment promotes bioplastics such as PLA within national strategies to reduce reliance on conventional plastics.
At the global level, the United Nations Environmental Programme and related international bodies identify biodegradable polymers like PLA as key materials in worldwide efforts to reduce plastic pollution. UNEP’s plastics statistics framework emphasizes the importance of biodegradable and bio-based alternatives for improved circularity and responsible materials management.
Key process steps from lactic acid fermentation to PLA production
PLA production involves several tightly controlled stages:
- Fermentation: Carbohydrate‑rich feedstocks such as sugarcane, corn or agricultural residues are fermented by microorganisms to produce lactic acid. Lactic acid purity and concentration directly affect polymer quality and process stability
- Purification: The fermentation broth is purified using filtration, ion exchange and evaporation to remove water and impurities. Even trace contaminants can impair downstream catalyst performance
- Lactide synthesis: Purified lactic acid is converted into low‑molecular‑weight pre‑polymers and lactide. High optical purity is required to achieve the desired crystallinity and mechanical properties
- Polymerization: Lactide is polymerized via ring‑opening polymerization to form PLA, allowing control of molecular weight and polymer structure for applications such as packaging, fibers and 3D printing
- Process stability: Variations in pH, temperature, purity or composition across the production chain can reduce efficiency and increase energy demand. Stable operating conditions are essential for industrial‑scale PLA production
How process variability affects efficiency in PLA production
Process variability in lactic acid fermentation affects performance in ways that are not always immediately visible. Even within optimal operating ranges, small shifts in conditions can change how efficiently sugars are processed into lactic acid.
Reduced conversion at this stage alters lactic acid concentration and the overall composition of the fermentation broth. This increases the load on downstream purification and can interfere with polymerization efficiency. As a result, yield, throughput and final polylactic acid quality become inconsistent.
These effects originate from the interaction of multiple process parameters such as pH, temperature and substrate availability. When process parameters drift, the process gradually moves away from optimal conditions.
Without reliable visibility into these variables, operators cannot correct deviations at the point where they occur. This allows inefficiencies to build across the process and ultimately impacts overall production performance.
Typical outcomes from fermentation variability include:
- Declining lactic acid concentration at harvest: Signals incomplete sugar conversion, reducing yield and increasing production cost
- Increased formation of unwanted by-products: Lowers effective lactic acid yield and increases purification complexity, energy use and chemical consumption
- Slower fermentation cycles and longer batch times: Reduces reactor productivity and limits overall plant throughput
- Difficulty maintaining the target pH profile: Disrupts microbial metabolism, leading to fluctuating productivity and variable batch quality
- Oxygen ingression or inconsistent anaerobic conditions: Alters fermentation pathways, increasing by-product formation and affecting stereochemical consistency of PLA
- Unoptimized feed schedule: Causes inconsistent yields and lost batches
Early symptoms of a bioprocess excursion are often invisible to operators and rarely originate from a single process attribute. Instead, they reflect the complex biological processes that change and interact over time.
Common causes of fermentation instability include:
- pH instability affecting microbial metabolism and lactic acid productivity: Even small pH deviations alter enzymatic activity and reduce sugar‑to‑lactic‑acid conversion efficiency
- Temperature fluctuations that alter reaction kinetics and slow fermentation: Unstable thermal conditions affect microbial growth rates and extend fermentation time
- Unoptimized feed leading to variability and lost batches: Feed variability prevents steady metabolic activity and introduces batch‑to‑batch differences
- Oxygen exposure that disrupts anaerobic fermentation pathways: Oxygen ingress changes fermentation behaviour and increases by-product formation
- Foam formation that reduces effective reactor volume: Excessive foam limits usable fermentation volume and interferes with mass transfer
- Insufficient real‑time insight into lactic acid formation: Reliance on indirect indicators or delayed laboratory analysis can prevent early detection of deviations, allowing yield and quality losses to develop before corrective action is taken
Together, these factors show that fermentation performance depends on a small number of tightly linked variables. Maintaining stability requires continuous monitoring and precise control of these parameters. Defining the right measurement points is therefore essential for effective PLA process quality control, ensuring consistent output and efficient production at scale.
Key measurement points for reliable PLA process quality control
Efficient PLA production depends on accurate monitoring and control of key variables across fermentation and downstream preparation. Lactic acid fermentation is highly sensitive to biological and thermal variation, making measurement essential for maintaining stable operating conditions. The following measurement points are critical for achieving effective PLA process quality control and ensuring consistent performance across the production chain.
Feed control
- Flow measurement of sugar, nutrient and buffer feeds stabilizes substrate availability and prevents overfeeding or starvation that disrupts microbial metabolism
- Density or concentration monitoring of feed streams helps detect variations in raw material quality and supports substrate concentration control
- Feed temperature monitoring ensures substrates enter the bioreactor within the appropriate thermal range to avoid metabolic stress
Fermentation control
- pH measurement is critical for maintaining optimal microbial activity and protecting lactic acid productivity throughout the batch
- Temperature monitoring stabilizes fermentation kinetics and prevents yield losses caused by thermal deviation
- Turbidity or biomass measurement, combined with lactic acid concentration monitoring data, provides visibility into microbial growth patterns and early indication of declining fermentation performance
- Pressure monitoring supports controlled CO₂ release and highlights gas accumulation or restriction in exhaust paths
- CO₂ monitoring, while optional, provides additional insight into metabolic activity and fermentation progression
- Nutrient and metabolite monitoring is essential for achieving process yield targets consistently from batch to batch
Purification control
- Conductivity monitoring detects residual salts or ionic impurities that influence downstream purification performance
- Broth chemical composition reveals bulk material composition and major impurities
- Flow measurement stabilizes transfer conditions and supports consistent feed to purification units
Polymerization control
- Temperature measurement during lactide formation and polymerization maintains stable reaction kinetics and prevents uncontrolled transesterification or degradation
- Vacuum monitoring and control ensures efficient removal of water and low‑boiling components
- Target molecule measurement provides real-time composition and molecular structure attributes
Impact of robust measurement solutions on PLA fermentation yield
Reliable measurement is the difference between a fermentation process that reacts to problems and one that consistently delivers high yield. When key process variables are measured accurately and continuously, operators gain the ability to keep lactic acid fermentation within its optimal operating window. This prevents small deviations from accumulating and protects yield, batch duration and downstream performance across PLA production.
Accurate measurement data supports:
- Lower production cost per kilogram, due to reduced by-product formation, lower waste generation and improved resource efficiency
- Reduced chemical consumption, including neutralizers, buffers and nutrients, achieved through tighter pH control
- Fewer unplanned shutdowns and batch failures, supported by early detection of deviations and improved anaerobic control
- Lower downstream processing effort, as consistent broth composition reduces filtration load and purification intensity
- Improved operational efficiency, with shorter cycle times, higher plant utilization and controlled batch durations
- Reduced safety and compliance risk, through improved visibility into oxygen ingress, CO₂ release and pressure behaviour, supporting PLA recycling and circularity goals
Key questions in polylactic acid (PLA) process control
The following questions address how upstream deviations, measurement strategies and operating choices influence lactide synthesis, polymerization performance and overall process stability. Together, they highlight the key levers for industrial‑scale PLA production.