尝试输入关键词、订货号/产品型号或序列号(“CM442”或“技术资料”)进行查找
至少输入2个字符开始搜索。
Polymerization plant

Sensors for the chemical industry

State-of-the-art sensors for chemical plants ensure accurate measurements, increase operational efficiency and lower long-term maintenance costs

Outdated technology can compromise both production processes and availability. Older measuring technologies leveraging mechanical components are less accurate and require higher levels of maintenance than modern equivalents in order to ensure production. Investing today to replace old mechanical devices with innovative sensor technology will pay dividends in the long run, both in productivity gains and maintenance cost savings.

How we can help

Irrespective of the chemical industrial process or application, the latest generation of Endress+Hauser sensors will enable you to hit your productivity and cost targets, providing accurate measurements, reducing maintenance and downtime during calibration and proof testing. Moreover, our sales and service teams are available worldwide for end-to-end support, from selecting the appropriate sensors to replace old devices, to designing custom maintenance concepts.

  • Safe in-process cleaning and calibration plus self-diagnostics and effortless proof testing through smart instrumentation with integrated Heartbeat Technology

  • Advanced diagnostics for unplanned shutdown prevention

  • Directly available mobile field data with RFID tags for fast access to asset information

  • Unified platforms in transmitters to support a reliable, focused maintenance approach

  • Best-fit instruments with intrinsic safety and high accuracy providing reliable data and process safety

应用

Measure polymerization viscosity efficiently

Viscosity is a crucial fluid property and a fundamental measurement parameter in polymerization process control. As a variable, it can be used to monitor product quality. Older viscosity measuring devices using mechanical components require regular maintenance to ensure filters are kept clear and production is running.

Polymerization viscosity measurement with Promass I
我们的行业专业知识

The Endress+Hauser Coriolis Promass I flowmeter offers multiple benefits over older mechanical devices for peak performance at reduced operational costs.

  • No filter required, meaning significant time and cost savings in maintenance with sustained process performance and safety

  • Optimize product quality with a single measuring point. In-line multivariable measurement of flow, density, temperature and viscosity

  • Minimize pressure loss with a straight, single-tube design

Prolong sensor lifetimes

In Olefin, quenching pH measurement of the contaminated quench water at regular intervals can go a long way to helping prevent fouling in the bottom of the tower. Cleaning sensors at least every other day is required, a time-consuming and labor-intensive activity which, if left undone, can result in their needing to be replaced every two weeks.

Liquiline Control CDC90 for automatic cleaning of pH sensors
我们的行业专业知识

The Endress+Hauser Liquiline CDC90 extends the lifetime of your sensor more than thirtyfold.

  • Save time with in-process cleaning and calibration with no electrode removal necessary

  • Spur efficiency with self-diagnostic systems such as sensor conditioning checks

  • Foster safety for people and processes as no handling of contaminated water is needed

Prevent unplanned shutdowns

Use of old, magnetic level gauge devices during olefin fractionation in high-temperature environments can reduce safety and result in unreliable measurements. Moreover, unplanned shutdowns can occur if the temperature gets too high.

Chemical facility
我们的行业专业知识

The Endress+Hauser Levelflex FMP51 guided wave radar ensures controlled, reliable fractionation.

  • Measure levels remotely, continuously and reliably in high-temperature conditions based on the time-of-flight principle

  • Avoid unplanned shutdowns by detecting false trips which create the risk of a stuck device

  • Enhance safety with a second unit connected to the Safety Instrumented System (SIS)

What you can do

Click through these process maps and learn how you can reduce maintenance costs in your chemical plant!

Process map of a batch reactor in the chemical industry ©Endress+Hauser

With modern technologies you keep your polymerization reactor under control.

Process map of ethylene production ©Endress+Hauser

Modernizing your ethylene production ensures a smooth process with reliable data to enhance productivity and to prevent unplanned shutdowns.

Process map of an olefin quenching tower ©Endress+Hauser

A reliable pH measurement at regular intervals of the quenching water requires cleaning of the sensor at least every other day, which takes up a great deal of effort in terms of time and people.

Process map of fractionation in the olefin process ©Endress+Hauser

Decreased process control creates unreliable fractionation – for example, remote control cannot be done with outdated technology for level measurement.

Meet our expert

“以我的经验,只有将维护成本降至最低才能降低您的工厂的总运营成本。”

Gustavo Stasiejko

行业经理, Endress+Hauser集团服务

优势

With 60+ years of application know-how in chemical industries, we stand for a long-lasting relationship with our customers. With your benefits in mind, we make sure you get the necessary support to optimize your processes, from choosing the right sensor through to maintenance concepts. The basis for your success is our global service and sales force located in your region and standing by your side as trusted experts.

  • 13,000

    employees worldwide

  • up to 130,000 €

    cost savings per year in the maintenance of your pH electrode, when using our Liquiline automated cleaning and calibration system, considering 10 measuring points in your plant

  • 650,000+

    Coriolis flowmeters successfully installed

  • 简易产品

  • 轻松执行仪表选型、安装和操作

仪表技术性能

选型便捷程度

  • 标准产品

  • 测量可靠、坚固耐用、低维护需求

仪表技术性能

选型便捷程度

  • 高端产品

  • 功能丰富,适用范围广

仪表技术性能

选型便捷程度

  • 定制产品

  • 专门针对严苛工况设计

仪表技术性能

选型便捷程度

特殊选型

FLEX产品选型 仪表技术性能 选型便捷程度
  • F
  • L
  • E
  • X

Fundamental选型

完美胜任基本测量任务

仪表技术性能
选型便捷程度
  • F
  • L
  • E
  • X

Lean选型

轻松应对关键工艺的测量挑战

仪表技术性能
选型便捷程度
  • F
  • L
  • E
  • X

Extended选型

创新技术助力工艺流程优化

仪表技术性能
选型便捷程度
  • F
  • L
  • E
  • X

Xpert选型

满足严苛工况的特殊测量要求

仪表技术性能
选型便捷程度

特殊选型

浏览我们的产品系列!

相关案例

其他行业