Title

Hãy thử tìm kiếm theo từ khóa, đơn hàng hoặc mã sản phẩm hoặc số sê-ri, ví dụ: “CM442” hoặc “Thông tin kỹ thuật”
Nhập ít nhất 2 ký tự để bắt đầu tìm kiếm.
  • Lịch sử

Complete Emissions monitoring equipment at Germany's first liquefied natural gas terminal

Ngành công nghiệp: Dầu khí
Top-down view of an LNG tanker ship transporting liquefied natural gas (LNG) at sea

Vui lòng cho chúng tôi biết làm thế nào chúng tôi có thể hỗ trợ bạn tốt hơn. Bằng cách đó, chúng tôi có thể liên hệ lại với bạn cùng với câu trả lời tốt nhất có thể.

Tóm tắt

The events of 2022 sent shock waves through the energy market. All of a sudden, liquefied natural gas has become a hot topic in Germany‚ too. The system for measuring flue gas at Germany’s first LNG terminal in Wilhelmshaven is provided by SICK (now marketed by Endress+Hauser).

The results:

  • Since mid-December 2022, Germany has been operating its own liquefied natural gas (LNG) terminal in the form of the Höegh Esperanza, a ship docked in Wilhelmshaven.
  • For emission monitoring, a new system had to be designed for this special application: In addition to the special requirements on explosion prevention, German federal emissions legislation for large combustion plants applies to the ship instead of the requirements of the International Maritime Organization because it is in port for more than ten days.
  • This article was first published on www.sick.com on April 27th, 2023. Since Jan 1st 2025 Endress+Hauser exclusively markets SICK’s gas analysis and flow measurement technology worldwide.

Since mid-December 2022, Germany has been operating its own liquefied natural gas (LNG) terminal in the form of the Höegh Esperanza, a ship docked in Wilhelmshaven. It is due to feed around five billion cubic meters of natural gas into the German gas grid every year. That amounts to roughly 6% of gas demand in Germany. The federal government organized the Floating Storage & Regasification Unit (FSRU) within a very short space of time as a means of rapidly reducing Germany’s dependence on single sources of energy, especially Russian gas. The Höegh Esperanza has been chartered for ten years to regasify the natural gas that is liquefied at –163 degrees Celsius for transportation on tankers. On board the FSRU, steam is generated and used to heat the liquefied gas. Once it has reverted to its gaseous state, it is routed to the gas metering station, where it undergoes fiscal metering before being passed to the operator of the gas grid. The fact that Endress+Hauser equipment is used for the fiscal metering of the gas delivered by the Höegh Esperanza will come as little surprise.

The customer requirement: Emission compliance under stricter regulations

What is special about Germany’s first FSRU is that the emissions released by the regasification process are likewise measured with proven SICK technology. “We have developed an entirely new technical system for this special application, which had not previously existed in this form,” explains Markus Haas, Industry Manager Power & Energy at Endress+Hauser SICK. “In addition to the special requirements on explosion prevention, German federal emissions legislation for large combustion plants applies to the ship instead of the requirements of the International Maritime Organization because it is in port for more than ten days.”

Complex project with a large number of players

It is a challenging project, not only because of these requirements but also because of the multitude of international players involved, from the shipyard and the vessel’s owner to the authorities and various SICK offices in place such as South Korea, Japan and Norway. “This international approach and the coordination involved made the project extremely dynamic and complex,” says Anette Schultis, Head of International Account & Project Consulting at SICK AG. Then there was the intense time pressure. Owing to the tricky situation surrounding the supply of gas, everything had to happen very quickly, as we will all doubtlessly be aware. “The system was commissioned in 2022. The installation of the flanges and other preparatory work took place in October 2022 while the Höegh Esperanza was docked in Brest.” says Schultis.

Our solution:

The fact that SICK was in the right place at the right time was helped by the company having previously been in contact with Uniper, the operator of the terminal. The first inquiries about emissions monitoring equipment for flue gases at liquefied natural gas terminals were made back in 2016. In 2019, SICK worked with the boiler manufacturer, engine manufacturer and emissions experts from SICK to draw up a plan for monitoring eight sampling sites on board an FSRU in accordance with emissions regulations.

When receiving Uniper’s inquiry for the Höegh Esperanza in spring 2022, these plans worked to its advantage, even though the ship naturally had completely different technical specifications. “This preliminary work, our expertise and the fact that we have a suitable product in the MCS200HW all lent us the momentum needed to deliver our solution in good time,” says Haas. The emissions monitoring system went into operation on the Höegh Esperanza in May 2023 following the transition period for emissions monitoring.

Preparing for green gas

Although in the case of the Höegh Esperanza, a supply of natural gas was set up on short notice and a clean means of controlling emissions was implemented, LNG is still regarded as a transitional fuel as far as climate change mitigation is concerned. Consequently, it is to be ensured in the future that FSRUs are suitable for zero-carbon energy generation; for example, by regasifying liquid ammonia. But the team had already factored that into its solution. “The system requires only minor modifications to be used for ammonia further down the line,” says Haas.

This is an important aspect that makes the emissions monitoring system for the Höegh Esperanza a key project that will be very significant in showing what the way ahead will look like – and one with enormous potential.

Liên hệ với chúng tôi

Bạn quan tâm đến dịch vụ cung cấp của chúng tôi? Bạn có muốn thảo luận về ứng dụng của mình không?

Vui lòng cho chúng tôi biết làm thế nào chúng tôi có thể hỗ trợ bạn tốt hơn. Bằng cách đó, chúng tôi có thể liên hệ lại với bạn cùng với câu trả lời tốt nhất có thể.

Products and services used

/

Related solutions and technology

Emission monitoring solutions

Benefit from our decades of experience and a complete portfolio for continuous emission monitoring, with future-orientated solutions tailored to the respective measuring task in your industry.

Thông tin bổ sung

Ultrasonic flowmeters

Proline Prosonic Flow and FLOWSIC ultrasonic sensors guarantee versatile and economical measurement of gases and liquids up to a nominal diameter DN 4000 (156")

Thông tin bổ sung

Custody transfer of LNG: how latest ultrasonic measurement technologies support the accuracy needed

Discover how recent advancements in ultrasonic measurement technology improve custody transfer accuracy, reduce uncertainty, and support reliable trading across the LNG value chain.

Thông tin bổ sung

FAQs

Company logo of: Höegh Evi

Höegh Evi is a global leader in floating energy infrastructure, securing energy supply in times of crisis and meeting long-term energy needs. Höegh Evi delivers fast, adaptable, and secure solutions that respond to countries’ evolving energy needs. Höegh Evi has one of the largest and most technically advanced FSRU fleets in the industry. To date, they have owned and operated eight LNG carriers, successfully built ten FSRUs, and safely completed more than around 12,000 ship-to-ship operations.