Title

Hãy thử tìm kiếm theo từ khóa, đơn hàng hoặc mã sản phẩm hoặc số sê-ri, ví dụ: “CM442” hoặc “Thông tin kỹ thuật”
Nhập ít nhất 2 ký tự để bắt đầu tìm kiếm.
  • Lịch sử

Increasing reference meters' availability

External management improves operational quality

For this biotechnology plant, Endress+Hauser is the single point of contact to perform the management of the reference standards. The significant reduction of non-conformities achieved has led to better operational quality. Thanks to higher availability and obsolescence management of the reference standards, the site has gained in productivity.

calibration management, operational quality, increasing reference meter availability ©Endress+Hauser

More than 100 reference meters are managed and calibrated per year.

Benefits at a glance

  • 10 times less time spent internally on managing non-conformities

  • Significant reduction of overall costs

  • More than 90% availability achieved

  • Improved service quality at optimized cost

The challenge

The management of the calibration of the more than 100 reference standards covered about 20 calibration service providers. Facing the lacks in standardization and in the harmonization of the calibration specifications, people struggled to manage the due dates and lost a lot of time performing non value-added activities. As a result, on average over the year, reference meters were unavailable for over two months.

Our solution

Endress+Hauser took the responsibility to manage the whole calibration process of the reference standards, including:

  • A planning that ensures the availability of standards according to the site’s requirements

  • Sub-suppliers’ qualification and management

  • The complete logistics around the service

  • A check of the data received from the suppliers

  • A follow-up of the identified drifts

Liên hệ chúng tôi

Bạn quan tâm đến dịch vụ cung cấp của chúng tôi? Bạn có muốn thảo luận về ứng dụng của mình không?

Vui lòng cho chúng tôi biết làm thế nào chúng tôi có thể hỗ trợ bạn tốt hơn. Bằng cách đó, chúng tôi có thể liên hệ lại với bạn cùng với câu trả lời tốt nhất có thể.