![](/__image/a/1207081/k/da010a359316d19fa10c993b828b021ea45c1fca/ar/1-1/w/100/t/jpg/b/ffffff/fn/Martin%20Raab.jpg)
Martin Raab
Head of Public Communication and Group Media Spokesman, global
The company was recognized during Frost & Sullivan’s awards gala in California. “Endress+Hauser’s success is tied to a strong customer focus and a high level of innovation,” says Dr. Rajender Thusu, Frost & Sullivan Industry Analyst. The company invests heavily in research and product development in order to meet its customers’ requirements in the area of liquid flow measurements.
Frost & Sullivan highlighted the company’s close collaboration with customers. “Our aim is to help our customers run their processes in a reliable, safe, sustainable and economic manner. To do that, we work closely together with the customers from the very early stages of product design, to the operations phase and beyond,” says Dr. Bernd-Josef Schäfer, Managing Director of Endress+Hauser Flowtec, the Group’s competence center for flow measurement technology in Reinach, Switzerland.
The Endress+Hauser product portfolio of electromagnetic flowmeters guarantees precise measurement of volume flow without restricting production flow rates or causing any pressure drop. The result is less downtime and increased productivity, which contributes to lower overall operational costs. “Most of our customers value the combination of state-of-the-art electromagnetic flow measurement instruments and the wide range of services that we offer,” emphasizes Bernd-Josef Schäfer.
Apart from the extensive portfolio of measurement instruments, Endress+Hauser also offers global support services that enable customers to optimize their processes over the plant’s entire life cycle, thus making the company more competitive. This includes calibration, diagnosis, repair, engineering, commissioning and maintenance services.
The electromagnetic flowmeters from Endress+Hauser, which feature advanced engineering such as Heartbeat Technology, support various communications protocols, including EtherNet/IP and PROFINET, that make the information easily accessible.
Thanks to Heartbeat Technology, instruments such as the Proline flowmeter line have self-monitoring capabilities. By supplying process and instrument diagnostic notifications in line with NE 107, influences and changes can be detected and rectified before impacting the process – all while the process is running.
Cỡ tập tin: |
26.4 MB |
Tên tập tin: |
EH_2018-03_07_Market Leadership Award.zip |
Nhận trực tiếp các thông cáo báo chí và tin tức kế tiếp trong hộp thư của bạn. Cập nhật thông tin bằng cách đăng ký danh sách báo chí Endress+Hauser.
Martin Raab
Head of Public Communication and Group Media Spokesman, global