Title

Hãy thử tìm kiếm theo từ khóa, đơn hàng hoặc mã sản phẩm hoặc số sê-ri, ví dụ: “CM442” hoặc “Thông tin kỹ thuật”
Nhập ít nhất 2 ký tự để bắt đầu tìm kiếm.
  • Lịch sử

Industrial energy management: From measurement to EnPIs

Enhance energy transparency in manufacturing with reliable utility consumption monitoring, actionable energy performance indicators and measurement data that enables continuous improvement

Two engineers wearing harnesses discussing in front of wind park with cloudy sky

Why energy management starts with measurement, not targets

Rising utility costs, sustainability expectations and production efficiency targets are putting new pressure on industrial operators to understand where energy is consumed and where it can be saved. But an energy target without reliable measurement remains an estimate.

Industrial energy management starts with transparent data from the plant floor. By measuring utility consumption across relevant processes, plants can identify significant energy users, compare performance over time and act on deviations before they become recurring losses. Reliable measurement creates the foundation for energy efficiency monitoring, energy reporting and a structured energy management strategy

What an industrial energy management plan actually contains

An industrial energy management plan defines how a plant measures, manages and improves energy performance over time. It should connect four core elements:

  • Measurement points define where energy and utility consumption are captured, from incoming supply to major consumers such as boilers, compressors, chillers, heating and cooling systems.
  • Energy performance indicators, or EnPIs, translate raw consumption data into meaningful operating metrics, such as energy use per tonne produced, boiler efficiency or compressed air consumption per unit
  • An energy baseline provides the reference point for improvement. It allows teams to compare current energy performance against a defined period, normalized for production volume, ambient conditions or product mix.
  • A reporting scheme ensures that energy data does not remain isolated in instruments or systems. Regular review turns energy monitoring into energy management by linking measured variance to operational action.
Female engineer operating a device at a utility plant

How much can utility monitoring save? 5 to 15%, and what that depends on

Studies on ISO 50001 and building energy management systems show that systematic energy management typically delivers energy savings in the range of approximately 5% to 15%, with higher savings possible when supported by technical efficiency measures. This range depends on the current level of energy transparency, the number of utilities measured and the ability of plant teams to act on the results.

To make this saving potential measurable, plants need visibility beyond total site consumption. Incoming supply, utility generation and major energy-consuming areas should be monitored so that inefficiencies can be traced back to specific processes or systems.

Setting energy performance indicators that hold up

An energy performance indicator, or EnPI, is a measurable value used to track energy performance in relation to production, process output or operating conditions. A useful EnPI does not only show how much energy is consumed. It shows whether energy was used efficiently. Examples of industrial EnPIs include:

  • kWh per tonne produced for energy-intensive production lines
  • m³ of compressed air per unit produced for compressed air systems
  • kg of steam per batch for thermal processes
  • Specific energy consumption for comparing energy use across batches, lines or sites

The right EnPI should be continuously measurable, attributable to a defined process and normalized for output. This prevents teams from misreading higher consumption as poor performance when production volume, product mix or ambient conditions have changed. Reliable EnPIs depend on reliable measurement. If the meter behind the indicator is not accurate, the energy KPI will not support confident decisions.

Two engineers looking up at the piping of a dairy production unit ©Endress+Hauser

Where to install meters: Mapping tier-one and tier-two utilities

Tier-one utilities are primary resources purchased by a facility, such as electricity, water and natural gas. Tier-two utilities are generated on-site from these resources, such as steam, compressed air, heating and cooling, and are often the areas where significant energy-saving opportunities can be identified. Submetering in an industrial plant allows to measure energy consumption below the site level, for example at utility generation, process area or major equipment level. It helps teams move from total consumption figures to actionable information. A practical metering hierarchy starts with:

  1. Incoming supply to understand total site energy and utility consumption
  2. Tier-two utility generation, such as boilers, compressors, chillers or heating systems
  3. Largest consuming areas or production lines, where savings potential is most relevant
  4. Selected process-level consumers, where detailed EnPIs or benchmarking are required

For plants with limited budgets, a phased approach can help. In year one, focus on total consumption. In year two, extend measurement to the main consuming areas. In later phases, benchmark major consumers and production lines to identify recurring deviations and improvement opportunities.

Establishing an energy baseline you can defend

An energy baseline is the reference point used to evaluate whether energy performance has improved. It defines how much energy a process, line or site typically uses under comparable operating conditions.

A defensible baseline requires enough measured data to reflect normal production patterns. It should also be normalized against variables that influence consumption, such as production volume, ambient temperature, operating hours or product mix. Once a baseline is established, energy benchmarking becomes possible. Teams can compare similar lines, sites or operating periods and identify where performance deviates from expected energy use.

What ISO 50001 expects from your measurement data

ISO 50001 provides a framework for systematic energy management. From a measurement perspective, the standard requires organizations to understand their energy use, identify significant energy users and demonstrate improvement against a defined baseline.

Process instrumentation, utility metering and diagnostics that help create reliable, auditable measurement data for energy management and continuous improvement.

For companies preparing for ISO 50001 implementation, trustworthy measurement data supports three practical needs: identifying significant energy users, tracking EnPIs and providing evidence that energy performance is improving over time.

Is an industrial energy audit the same as ISO 50001?

An industrial energy audit is an assessment used to identify where energy is consumed and where efficiency improvements may be possible. ISO 50001 is a management system standard that helps organizations manage and improve energy performance continuously.

An audit can provide useful input for an energy management plan, but sustained improvement depends on ongoing measurement, monitoring and action.

Energy efficiency monitoring: Turning meter output into savings

Energy efficiency monitoring becomes valuable when measured data leads to action. The chain is simple: Measure consumption, aggregate data, normalize it against the energy baseline, detect deviations and decide what needs to change. Metered utility consumption also provides the activity data needed for sustainability reporting, supporting Scope 1 emissions calculations through fuel use in boilers and Scope 2 reporting through purchased electricity consumption.

For example, if compressed air consumption rises while production output remains stable, the variance may indicate leaks, pressure losses or inefficient operating settings. If steam use per batch increases, the cause may sit in distribution losses, process settings or heat transfer performance.

Energy reporting helps keep these insights visible. Regular reports allow operations, maintenance and sustainability teams to align on priorities, track progress and document the impact of implemented energy conservation measures.

Energy management in food and beverage production

Food and beverage production is often energy-intensive because many processes depend on thermal treatment, refrigeration, clean-in-place operations, compressed air, steam, heating and cooling. These utilities can represent major energy consumers and are often distributed across several production areas.

Industrial energy management helps food and beverage manufacturers identify where consumption is highest, which processes vary most and where efficiency improvements can be prioritized without compromising food safety, quality or uptime.

Keeping the data trustworthy: Instrumentation and diagnostics

An EnPI is only as reliable as the measurement behind it. Process instrumentation provides the field data needed to calculate energy performance, detect inefficient operation and verify whether improvement actions are working.

In-situ verification and diagnostics help maintain confidence in measurement data over time. Endress+Hauser Heartbeat Technology, for example, supports device verification and diagnostics without interrupting the process, helping plants keep energy data trustworthy throughout the instrument lifecycle.

Once the energy management plan, EnPIs and baseline are defined, the next step is to identify where the largest savings potential sits in the plant. Utility systems such as steam, boilers, heating and cooling as well as compressed air often provide practical starting points for improvement.

FAQ

Everything you need to know about industrial energy monitoring

Chú thích cuối

Find out more about our competences