Improve the safety of your steel production with our dedicated measurement and software offering
High temperatures, molten metal and heavy loads - steel production puts a lot of stress on both man and machine. So it is only natural that safety and availability are one of the top priorities for steel plant managers. Not only to prevent potentially deadly accidents from happening but also to make sure that production in a extremely competitive landscape never stops. For that you need robust measurement equipment that provides reliable data as well as smart control solutions.
1.63 mil.
tonnes of crude steel
were produced worldwide in 2016. This is an increase by 0,8% compared to 2015 according to the World Steel Association.
Comply with functional safety standards IEC/EN 61508 (process hazard categorization known as SIL - Safety Integrity Level) and IEC/EN 61511 (process safety using instrumentation known as Safety Instrumented Systems) in accordance with EN 13849 with process experts who guide you every step of the way in selecting the best-fit, industry-optimized instrumentation, service and solution package from our complete portfolio based on more than 60 years of experience.
Safe monitoring of critical cooling water circuits
Acid level measurement and overfill prevention
SIL certified instrumentation
Online monitoring of measuring points
Applications
Safe monitoring of critical cooling water circuits
Malfunctions in water circuits can be very dangerous to both equipment and personnel. Especially in a steel plant, where they are used to control the very high temperatures of various types of oxygen lance cooling in converters and wall and roof panels of electric arc furnaces. Also the quality of the water must be monitored regularly to prevent the growth of algae or even infectious bacteria like legionella.
Chuyên môn của chúng tôi trong lĩnh vực
The sensors to monitor these processes were developed to withstand the harsh conditions in a steel plant.
Our leakage detection solution measures the inlet and outlet flow rates of the circuit by means of suitable flowmeters, either electromagnetic or ultrasonic. The inlet and outlet temperatures are acquired from sensors mounted near the flowmeters.
The water quality of the cooling circuit is controlled by monitoring parameters like pH, silicate build-up and oxygen. Our portfolio for liquid analysis including digital sensors and transmitters enables a reliable measurement.
Creating high-grade metal sheets includes pickling. This process step uses different kinds of acids to remove impurities. Handling these acids poses an environmental challenge and a safety issue. Above all, the acid storage tanks must be closely monitored to prevent an overfill.
Chuyên môn của chúng tôi trong lĩnh vực
Endress+Hauser offers radar level instruments which are specifically designed to withstand aggressive media and support you with the installation to produce reliable results. We also offer a complete overfill protection automation solution which will help you fulfill prevention requirements and save you time and money.
Process control is only as good as the instruments being used. To assess a sensor, operators can rely on industry standards such as the IEC 61511. It describes Safety Integrity Levels (SIL) that are an established benchmark for the safety integrity of a system.
Chuyên môn của chúng tôi trong lĩnh vực
Endress+Hauser has one of the most extensive portfolios of IEC 61508 certified instruments created according to safety by design standards. For hard- and software development, we have implemented standardized measures to avoid systematic faults and control random failures. Find our more about our SIL portfolio.
Online monitoring of measuring points
One of the basic ways to improve the safety of the employees is to reduce the time they spend in hazardous areas.
Chuyên môn của chúng tôi trong lĩnh vực
New online and digital measurement technologies enable you to control your processes remotely. Endress+Hauser has developed various digital services to support your operations.
Find out more about our Netilion digital servicesand our industrial tablets for convenient monitoring and configuration.
Find out how you can improve plant safety and availability
Lợi ích
Safety and plant availability are sensitive topics that demand a partner that you can trust, who is not interested in short-term profits but in developing sustainable relationships. Look no further, because Endress+Hauser for more than 60 years has been a reliable partner to steel companies in over 100 countries. Our instruments and solutions - all designed along industry-specific requirements - are relied upon all over the world.
200,000+
temperature sensors installed in safety critical steel production processes worldwide.
55,000
smart sensors integrated in 65 digital optimization projects.
2.6 mil.
field instruments delivered to mineral&metals operations since 2007 alone.
Nước, đồ uống, sản phẩm sữa, hóa chất hoặc dược phẩm phải được phân tích hàng ngày. Chọn thiết bị phù hợp với nhu cầu nhất từ danh mục sản phẩm toàn diện của chúng tôi.
Lưu lượng kế
Lưu lượng kế
Nước, khí tự nhiên, hơi nước, dầu khoáng, hóa chất là một số chất lỏng phải được đo đạc mỗi ngày. Chọn lưu lượng kế phù hợp nhất với nhu cầu quy trình.
Mức
Mức
Đo mức liên tục và theo dõi điểm đo mức trong chất lỏng và khối chất rắn
Áp suất
Áp suất
Thiết bị mạnh mẽ để đo áp suất quy trình, chênh áp, mức và lưu lượng.
Phần mềm
Phần mềm
Bên cạnh việc cung cấp các công nghệ về hệ thống và đo lường, chúng tôi cũng cung cấp các phần mềm phù hợp cho tất cả các ngành giúp tối ưu tiềm năng cho các quy trình vận hành.
Sản phẩm hệ thống
Sản phẩm hệ thống
Ứng dụng Applicator
Đo nhiệt độ
Đo nhiệt độ
Nhiệt kế và thiết bị truyền tín hiệu cho ngành quy trình
Câu chuyện liên quan
An toàn
Safety in mining industry enhanced, performance sustained
Make mining safer whilst guaranteeing performance using SIL compliant and digital instrumentation.
Endress+Hauser is dedicated to helping you meet your operating targets throughout the water cycle by combining an innovative portfolio of measuring instruments, expert services and industry expertise.
Food & Beverage: Trust in quality
Food & Beverage: Trust in quality
Your partner to meet global hygiene regulations, ensure consistent product quality and plant availability while conserving resources and lowering costs.
Power & Energy: Empower the future
Power & Energy: Empower the future
You provide the world with energy - we provide you with application know-how for your power plant including: steam, combined cycle power plants, waste-to-energy, hydroelectric and power-to-gas.
Chúng tôi tôn trọng quyền riêng tư của bạn
Chúng tôi sử dụng cookie để nâng cao trải nghiệm duyệt web của bạn, thu thập số liệu thống kê để tối ưu hóa chức năng của trang web và cung cấp nội dung hoặc quảng cáo phù hợp.
Bằng cách chọn "Chấp nhận tất cả", bạn đồng ý với việc sử dụng cookie của chúng tôi.
Để biết thêm chi tiết, vui lòng xem lại Chính sách cookie của chúng tôi.