One such term frequently associated with digitalization strategies is digital twin. The question is whether this concept is already a practical reality or just another marketing phrase. What are digital twins?
Article05.01.2026
Tóm lại
The term digital twin is widely used in discussions about industrial digitalization, often raising questions about whether it represents a genuine technological advancement or simply a buzzword.
In reality, digital twins are an established concept with significant practical applications.
A digital twin is a virtual representation of a physical asset, continuously updated with latest data to reflect its current condition.
In industrial environments, digital twins improve operational efficiency, support maintenance, and enhance decision-making by providing accurate insights into equipment performance.
This technology is no longer theoretical - it is a proven solution delivering measurable benefits across various sectors.
Mục lụcMục lục
What is a digital twin?
A digital twin is a digital representation of a physical product, process, or service. Through an online connection between the physical asset and its digital counterpart, analyses can be performed to monitor health conditions and prevent potential issues.
Digital twins also enable simulations, allowing process optimization, reduction of unscheduled downtime, and other improvements. While the concept is not new, it has gained prominence with the rise of IIoT and AI technologies.
There are multiple ways to implement digital twins in industrial applications. For example, a digital twin can be created automatically when field devices are connected to IIoT ecosystems via an edge device. Alternatively, it can be generated manually by scanning a serial number, uploading a photo, or entering data through a smartphone.
How do digital twins work?
In most implementations, the digital twin collects data from connected devices, analyzes it, and provides actionable insights. Development typically involves applying statistical methods, machine learning, and other advanced algorithms to interpret device performance and operational behavior.
Each asset is assigned a digital twin. This is achieved by connecting devices through a network - e.g. PROFIBUS - linked to an edge device that communicates with a cloud-base IIoT ecosystem. When the connection is established, digital twins are automatically created, ensuring accurate replication of physical assets and continuous data collection.
Depending on the IIoT platform, digital twins can be used for various purposes, such as analyzing installed bases, identifying obsolete devices, and recommending improvements.
Digitalization enables smart devices to generate large volumes of valuable data continuously. Manually interpreting this data is impractical, and ignoring it means losing critical insights into applications. A digital twin addresses this challenge by integrating with technologies such as artificial intelligence, machine learning, and IIoT, allowing simulations based on data from physical assets.
Digital twins collect and analyze information autonomously, providing actionable insights, which can help to improve processes or increase plant availability. Companies are increasingly developing open platforms to expand digital twin solutions that interpret data from connected devices. These insights are typically presented through dashboards for easy evaluation, eliminating the need for specialized data expertise
Why is the digital twin important to IIoT?
IIoT relies on smart devices that continuously deliver operational data, unlike traditional standalone systems. By connecting these devices to a cloud platform, digital twins create virtual representations. Combined with analytics tools, this approach transforms raw data into clear, actionable insights for the entire team. Applications include installed base analysis, performance improvement, and maintenance optimization.
Example of a digital twin application
Digital twin technology can be experienced through digital services such as Netilion Analytics, which enables users to register and organize assets in the Netilion IIoT ecosystem. This solution provides insights into the installed base, identifies obsolete devices, and highlights opportunities for standardization and process improvement.
Asset registration can be performed in several ways. The most automated method involves connecting the network to the IIoT ecosystem via an edge device, allowing digital twins to be created without manual input. Alternatively, assets can be added manually through the platform by entering device information or by using the smartphone app Netilion Scannerto scan devices, capture images, and record location details.
Once registered, the system offers analytics and insights, including asset diversity, criticality, and obsolescence, all accessible through a centralized dashboard.
Netilion is an award-winning IIoT ecosystem, designed for industrial processes. It connects the physical and digital worlds to send valuable information from the field to you anywhere at any time.
Actual hands-on tasks will help you to understand how the EtherNet/IP technology works in detail. You will understand the benefits of the technology and know the procedure for troubleshooting.
Would you like to participate at one of our events? Select by category or industry.
Chúng tôi tôn trọng quyền riêng tư của bạn
Chúng tôi sử dụng cookie để nâng cao trải nghiệm duyệt web của bạn, thu thập số liệu thống kê để tối ưu hóa chức năng của trang web và cung cấp nội dung hoặc quảng cáo phù hợp.
Bằng cách chọn "Chấp nhận tất cả", bạn đồng ý với việc sử dụng cookie của chúng tôi.
Để biết thêm chi tiết, vui lòng xem lại Chính sách cookie của chúng tôi.