Title

Hãy thử tìm kiếm theo từ khóa, đơn hàng hoặc mã sản phẩm hoặc số sê-ri, ví dụ: “CM442” hoặc “Thông tin kỹ thuật”
Nhập ít nhất 2 ký tự để bắt đầu tìm kiếm.
  • Lịch sử

Liquid analysis in LNG trains

Complete solution out of one hand

In gas liquefaction plants, many parameters must be monitored to ensure the safety of the plant and the employees. The different process areas place different demand on the liquid analysis. This demanding area requires the highest level of process expertise and know-how.

Gas pipes and tanks. ©Shutterstock

Benefits and results

  • Complete solution from one source, which greatly simplifies operation

  • Plant operators benefit from state-of-the-art sensor and analysis technology like Memosens technology

  • Endress+Hauser is a solution partner with comprehensive know-how even for such complex applications

Customer challenge

In order to transport gas efficiently over long distances, the LNG liquefaction of natural gas is a common process. However, since natural gas is very fragile and highly flammable, safety precautions must be taken to protect the surroundings and the environment. Different limit values must therefore be complied with during the various process steps in a gas liquefaction plant. Due to the complexity of the plant, numerous measuring points must be installed and maintained.

Our solution

One part of the process is sulfur recovery. In the Sulfur Recovery Unit (SRU), the pH values in the waste heat boilers must be monitored in order to act immediately in case of events that can be recognized by the change in the pH value. This is done with a sampling system due to the pressure. The pH value is also an important parameter in the area of large boilers. Carbonite solution is used in the cleaning process. To treat the solution, the conductivity is monitored in the scrubber system.

Liên hệ chúng tôi

Bạn quan tâm đến dịch vụ cung cấp của chúng tôi? Bạn có muốn thảo luận về ứng dụng của mình không?

Vui lòng cho chúng tôi biết làm thế nào chúng tôi có thể hỗ trợ bạn tốt hơn. Bằng cách đó, chúng tôi có thể liên hệ lại với bạn cùng với câu trả lời tốt nhất có thể.