Title

Hãy thử tìm kiếm theo từ khóa, đơn hàng hoặc mã sản phẩm hoặc số sê-ri, ví dụ: “CM442” hoặc “Thông tin kỹ thuật”
Nhập ít nhất 2 ký tự để bắt đầu tìm kiếm.
  • Lịch sử

TECOSOL achieves stable biodiesel production with robust instrumentation

Reliable measurement technology stabilizes processes under variable operating conditions

Ngành công nghiệp: Hóa chất
Biodiesel production process: stable operation with integrated measurement technology

Vui lòng cho chúng tôi biết làm thế nào chúng tôi có thể hỗ trợ bạn tốt hơn. Bằng cách đó, chúng tôi có thể liên hệ lại với bạn cùng với câu trả lời tốt nhất có thể.

Tóm tắt

TECOSOL is one of the leading biofuels manufacturers in Europe. They operate 2 plants and produce biofuel that achieves significant CO₂ savings compared to fossil diesel. Highly contaminated residues and waste materials, fluctuating feedstock compositions, high temperatures and vacuum conditions place demanding requirements on biodiesel production processes and instrumentation. Using the complete product portfolio from Endress+Hauser, TECOSOL GmbH operates a highly automated plant in Wittenberge that ensures cost-efficient, safe and stable production.

Ralf Türck, managing director of Tecosol

“With biodiesel from the new plant in Wittenberge, TECOSOL achieves over 90% CO₂ savings compared to fossil diesel. It represents one of the few effective solutions for decarbonization."

Ralf Türck, Managing Director, TECOSOL GmbH

The challenge: biodiesel production under feedstock variability and demanding process conditions

TECOSOL GmbH produces biodiesel from contaminated residues and waste materials generated, for example, in the timber industry and oleochemistry. The composition of these feedstocks varies significantly, requiring sophisticated process engineering. Safe control of high-temperature and high-pressure processes is required for the production of high-quality biofuel.

Storage and loading also present significant challenges. The tank farm must accurately record all inventories and correctly reflect storage and handling processes. It also needs to ensure transparent custody transfer subject to legal metrology for all material flows. The company’s goal was to realize a highly automated plant for continuous product and process monitoring even under variable raw material flows and complex process conditions.

Our solution: engineered instrumentation for reliable biodiesel production

From planning through to commissioning, TECOSOL GmbH, Endress+Hauser and the appointed project engineer worked in close partnership. Through intensive exchange and close coordination, the instrumentation was designed to meet the specific requirements of varying residues and waste materials, withstand high temperatures, pressures and vacuum conditions and be seamlessly integrated into the automation system.

Whether level, point level, flow, pressure or temperature, the complete product portfolio from Endress+Hauser covers all applications at the plant in Wittenberge, including analytical measurement technology and automation components.

Liên hệ với chúng tôi

Bạn quan tâm đến dịch vụ cung cấp của chúng tôi? Bạn có muốn thảo luận về ứng dụng của mình không?

Vui lòng cho chúng tôi biết làm thế nào chúng tôi có thể hỗ trợ bạn tốt hơn. Bằng cách đó, chúng tôi có thể liên hệ lại với bạn cùng với câu trả lời tốt nhất có thể.

Products and services used

/

Related solutions and technology

Temperature measurement

Thermometers and transmitters for the process industry

Thông tin bổ sung

Software solutions

Apart from all relevant measuring and system technologies, we also offer appropriate software for all branches of industry that provide to run your operating processes at its full potential.

Thông tin bổ sung

Pressure measurement

Pressure and differential pressure measurement for liquids, gases and vapors

Thông tin bổ sung

Level measurement

Continuous level measurement and point level detection in liquids and bulk solids

Thông tin bổ sung

FAQs

Company logo of: S-IU - PSR - Template

TECOSOL GmbH is one of Europe’s leading biofuel producers. Headquartered in Ochsenfurt, the company manufactures fuels that deliver significant CO₂ savings. At its Wittenberge site, TECOSOL has built a new biodiesel plant fully equipped with measurement technology from Endress+Hauser. The facility sets new standards for sustainable production and the circular economy.