Title

尝试输入关键词、订货号/产品型号或序列号(“CM442”或“技术资料”)进行查找
至少输入2个字符开始搜索。

Top 10 things to consider when installing a new pH loop

Selecting the correct sensor for your process

pH sensor installation ©Endress+Hauser

An example of a pH sensor installation in a convenient location for maintenance by plant personnel.

Are you looking to engineer the installation of a new pH loop, have a new loop ready for installation or re-doing an existing loop? Here is a roadmap to help you get past some of the most common road blocks.

This paper is written to help those who are looking to engineer the installation of a new pH loop, have a new loop ready for installation or are re-doing an existing loop. Whether a novice to the world of pH or a seasoned veteran, this is intended to be a helpful roadmap to a successful journey. It is not an end all be all, but rather a primer to get you past the most common road blocks.

Top 10 things to consider:

1. Watch your flow rate, pressure and temperature

2. Clean the sensor

3. Watch the temperature

4. Keep it wet and accessible

5. Consider redundancy

6. Monitor sensor life

7. Establish and follow QA/QC procedures

8. Handle sensors carefully

9. Use only as directed

10. Select the correct sensor for the process

One size does not fit all

It is important to work the manufacturer to select the pH sensor that will be best suited for your application. This is a case where one size does not fit all. Many manufacturers have their go-to sensor, a sensor that 80% of the time will cover most of the applications. That might be the sensor for you, or it might not.

联系信息

您对我们的产品组合感兴趣吗?想要谈谈您的实际应用吗?

请尽可能详细地告诉我们您的问题和需求,这样我们就能为您定制合适的解决方案了。