Title

尝试输入关键词、订货号/产品型号或序列号(“CM442”或“技术资料”)进行查找
至少输入2个字符开始搜索。

Waste-to-energy plant in Spain relies on proven technology for emission measurement

行业: 相关资源
TERSA's sustainable Waste-to-energy plant in Barcelona

请尽可能详细地告诉我们您的问题和需求,这样我们就能为您定制合适的解决方案了。

概述

A waste-to energy (WtE) plant in Sant Adrià del Besòs near Barcelona in Spain has rolled out an innovative system for ensuring better environmental practices. The plant is owned by the TERSA Group, a publicly owned environmental management company and designed for handling municipal waste. SICK Spain (now marketed by Endress+Hauser Spain) installed two measurement systems, doubling the reliability of the plant’s emissions data.

The results:

  • In line with the measures put in place by the local authorities to improve air quality, the TERSA Group aims to achieve the highest standards possible for efficiency and environmental sustainability. It believes that the new catalytic system installed in the WtE plant and driven by proven measurement technology is a key part of its efforts.
  • The project followed on from a public tendering procedure, which was won by PASCH, a Spanish company specializing in supplying and maintaining equipment.
  • This article was first published on www.sick.com on March 3rd, 2021. Since Jan 1st, 2025 Endress+Hauser exclusively markets SICK’s gas analysis and flow measurement technology worldwide.

The customer requirement: “We need the best emission monitoring solution available”

The plant has three waste treatment lines, with a maximum annual capacity of 360,000 tons, and annual production of 200,000 MW of electricity. “Because of where it is and what it does, the plant can potentially have a significant environmental impact. In order to ensure we meet levels set out in legal standards, we need the best emission measurement technology available”, explained Alessandro Leotta, Head of WtE at the TERSA Group.

Our solution:

With this goal in mind, the right environmental measurement equipment helps to improve process efficiency while minimizing the plant’s impact on the surrounding environment. This project involved a full analyzer system in the stack, along with a redundant system, designed to double the reliability of the data sent to the Catalonian authorities about the plant’s emissions.

These two pieces of equipment are made up of two MCS100FT multi-component Analyzers, two MERCEM300Z mercury Analyzers, two DUSTHUNTER SP100 particle Analyzers, two FLOWSIC100 gas flow measuring instruments, two MPR remote monitoring elements, and two control cabinets, along with a data handling system and another system used by both the plant and the local authorities to send the data. 

The equipment supply contract includes 24/7 maintenance, with a 4-hour response time. The system also has a remote monitoring service operated from Germany, which enhances the level of support.

During the lockdown caused by the COVID-19 pandemic, the MPR monitoring system has made it possible to diagnose faults, maintain the Analyzers, and manage alarms remotely, as well as the automated QAL3 settings. All of these features have contributed to helping the plant to keep operating and providing an essential service.

联系我们

您对我们的产品组合感兴趣吗?想要谈谈您的实际应用吗?

请尽可能详细地告诉我们您的问题和需求,这样我们就能为您定制合适的解决方案了。

Products and services used

/

Related solutions and technology

排放监测解决方案

为面向未来的排放监测提供广泛的产品组合和长期经验

更多信息

颗粒测量设备

环境的可持续保护有赖于对粉尘和颗粒排放物的检测和精确测量。

更多信息

超声波流量计

Proline Prosonic Flow 和 FLOWSIC 超声波传感器能够进行气体和液体测量,功能多,经济性好,最大标称口径为DN 4000 (156")

更多信息

过程气体分析仪

久经考验的测量技术,实现高效的过程控制

更多信息

企业商标 TERSA Group Waste-to energy plant

TERSA是 一家公有企业,业务遍及巴塞罗那都市区,专注于提供与循环经济相关的环境服务。公司通过各项业务,为废弃物管理、可再生能源的生产和商业化等挑战提供解决方案,同时倡导公众践行环保理念。TERSA集团由TERSA、SEMESA和SIRESA组成。