Title

尝试输入关键词、订货号/产品型号或序列号(“CM442”或“技术资料”)进行查找
至少输入2个字符开始搜索。

Prowirl with integrated pressure and temperature measurement

The vortex flowmeter for a transparent and cost-efficient energy management for steam and gas

发行日期: 04.01.2018

Pressure and temperature compensation – what for?

In the process industry, the pressure/temperature of steam/gases are often not constant. If such effects are not compensated, this leads to massive measurement errors and thus to energy and money losses. With the built-in (optional) pressure and temperature measurement, Prowirl 200 ensures the highest accuracy for determining the steam density and the energy content. The costly installation of four separate devices for flow, pressure, temperature and flow calculation is no longer necessary.

Picture of pressure ©Endress+Hauser

Wet steam detection – for higher safety and efficiency

Steam is used in large quantities in many applications (heating, cleaning or energy supply). But the heat transfer is only energetically efficient with “saturated steam.” But due to faults in the boiler system or existing condensate, “wet steam” often occurs in pipes with serious consequences: poor energy transfer, dangerous water hammers or harsh corrosion due dissolved salts. Prowirl 200 is the first vortex meter that is able to continuously monitor the steam quality and quantity.

picture of steam ©Endress+Hauser

Uniform two-wire concept

As an innovative two-wire measuring device, Prowirl 200 is based on a uniform device concept that significantly reduces the complexity for the user. The new concept standardizes operation, menu structures, function designations, software, interfaces, data management, system integration, error display, documentation, through to product structure. These innovations create long-term economic benefits for customers throughout the entire life cycle of their plant.

Worldwide unrivaled robustness

Prowirl 200 is the most robust vortex flowmeter available on the market. The capacitive DSC sensor ensures precise readings with the highest linearity even under the hardest process conditions. Thanks to its balancing, the DSC sensor is insensitive to system vibrations, temperature shocks (> 150 K/s) as well as water hammer and condensation-induced water hammers. Long-term test measurements confirm that Prowirl vortex meters have no drift even after decades of use (lifetime calibration factor).

下载

    从计量与监测到高级能源管理

    针对蒸汽生产、分配和消费等活动,我们了解能源与公用工程管理人员所面临的日常挑战和需求。

    蒸汽手册:蒸汽生产和蒸汽分配

    本手册旨在全面介绍各种形式的蒸汽,如何对其进行测量,以及在工业过程中能够利用蒸汽的场所及原因。

新闻列表

通过邮箱直接接收下一条新闻稿和新闻。订阅Endress+Hauser新闻列表,时刻关注最新动态。

Endress+Hauser press list

Endress+Hauser regularly sends out press releases on current topics and company information to media professionals.

Select the topics you are interested in:  *
Select the industries you are interested in: *

Personal Data


Fields marked with * are required. You will receive an email with a confirmation of your subscription. The information enlisted is voluntary and your data will only be used for personalizing your newsletters and not be passed onto any third party. For statistical reasons we will perform anonymous link tracking.