尝试输入关键词、订货号/产品型号或序列号(“CM442”或“技术资料”)进行查找
至少输入2个字符开始搜索。
  • 历史

Endress+Hauser acquires SensAction

Concentration measurement technology bolsters flow portfolio

发行日期: 14.03.2017

SensAction will operate as a division of the Endress+Hauser center of competence for flow measurement technology headquartered in Reinach, Switzerland. “This innovative technology is an excellent fit with our modern flow measurement portfolio,” says Dr Bernd-Josef Schäfer, Managing Director of Endress+Hauser Flowtec AG. “It allows us to further expand our range of products for measuring quality parameters.”

Already, Coriolis flow measurement devices from Endress+Hauser can determine not only mass flow, but density as well. Electromagnetic instruments are capable of measuring conductivity parallel to the volume flow. “These physical analysis parameters create direct value-add for the customer,” emphasizes Bernd-Josef Schäfer.

Endress+Hauser plans to integrate the SensAction instruments into its own program and open up new markets via the Group’s international sales structures. In addition, plans are in place to eventually combine the technology direct with Endress+Hauser flow instruments.

Innovative technology

The systems from SensAction measure the concentration of liquids with the help of surface acoustic waves, which are high frequency sound waves whose behavior can be compared to seismic waves created by earthquakes.

By analyzing the transmission time and amplitude, the acoustic parameters of the liquid, such as sound wave velocity, impedance and density, can be measured in order to quickly and precisely determine the concentration. Because they contain no moving parts, the systems are maintenance-free and do not suffer from wear-and-tear.

Apart from developing and manufacturing concentration measurement systems, SensAction also offers supplementary services, such as software products that rely on a laboratory measurement to provide a high degree of accuracy and user-friendliness for the customers’ applications. The key fields of application for the SensAction instruments include concentration measurements for liquid process media.

The acquisition of SensAction will be effective retroactively from 1 January 2017. Both parties have agreed to not disclose the details of the transaction. Stefan Rothballer and Michael Münch, two of SensAction’s founders, will continue to manage the innovative company’s business.

下载

    Endress_Hauser_SensAction_14-03-2017.zip

新闻列表

通过邮箱直接接收下一条新闻稿和新闻。订阅Endress+Hauser新闻列表,时刻关注最新动态。

Endress+Hauser press list

Endress+Hauser regularly sends out press releases on current topics and company information to media professionals.

Select the topics you are interested in:  *
Select the industries you are interested in: *

Personal Data


Fields marked with * are required. You will receive an email with a confirmation of your subscription. The information enlisted is voluntary and your data will only be used for personalizing your newsletters and not be passed onto any third party. For statistical reasons we will perform anonymous link tracking.

联系方式