Title

尝试输入关键词、订货号/产品型号或序列号(“CM442”或“技术资料”)进行查找
至少输入2个字符开始搜索。

Scaling Direct Air Capture for a net-zero future

DACMA's innovative carbon capture systems are designed to efficiently remove CO2 from ambient air. Reliable measurement from Endress+Hauser helps ensure process performance at scale.

行业: 相关资源
Containerized Direct Air Capture solution from DACMA

请尽可能详细地告诉我们您的问题和需求,这样我们就能为您定制合适的解决方案了。

概述

As industries work toward a climate-neutral future, technologies that actively remove carbon dioxide from the atmosphere are gaining importance. Direct Air Capture (DAC) offers a way to capture CO₂ directly from ambient air, creating new opportunities for carbon removal, utilization and storage. At the forefront of this innovation is DACMA, whose scalable DAC technology is designed to maximize CO₂ uptake while minimizing energy demand, helping transform ambitious climate goals into practical industrial solutions.

The results:

Verification

Every metric ton of CO₂ measured is quantifiable

Uptime

Every sensor failure is detected before it causes downtime

Process optimization

Every measurement feeds into real-time control of the plant

Digital twin

Every plant module is digitally mapped for predictive maintenance

Without precise measurement data, there can be no verifiable impact on the climate: Accurate tracking of energy consumption and CO₂ capture is key to the success of Direct Air Capture (DAC) systems - from regulatory approval to industrial-scale deployment. The measurement data from the plant provides DACMA with a clear basis for decision-making regarding the technology’s further development.

Adrian Kortmann, Project Manager at DACMA, in front of their containerized DAC unit

"As our systems evolve and scale, Endress+Hauser continues to support us with reliable instrumentation, technical know-how and a partnership approach that helps us tackle new challenges together."

Adrian Kortmann, Project Manager, DACMA GmbH
Frederik Effenberger in front of flow meter installed in containerized Direct Air Capture unit

"We are proud to support DACMA on their journey: With precise measurement technology, global expertise and a true partnership. For a climate-neutral future."

Frederik Effenberger, Industry Manager Decarbonization, Endress+Hauser

The challenge:

For Direct Air Capture (DAC) systems, process performance is defined not only by the amount of CO₂ captured, but also by the ability to quantify carbon removal with a high degree of accuracy. Reliable measurement data is essential for verifying capture rates, assessing process efficiency and establishing the transparency required by investors, regulators and carbon markets.

DACMA faced the challenge of measuring high-purity gaseous CO₂ under varying operating conditions while maintaining a compact system design. The instrumentation needed to deliver stable and accurate measurements without imposing complex installation requirements, ensuring seamless integration into the capture process.

Beyond CO₂ flow measurement, a comprehensive understanding of plant performance requires the correlation of multiple process variables, including pressure, temperature and energy consumption. Together, these parameters provide the operational insight needed to optimize capture efficiency, validate system performance and support the scale-up of DAC technology from pilot installations to industrial deployment.

Our solution:

Delivering process transparency and real-time data

To support accurate CO₂ quantification and energy monitoring, DACMA worked closely with Endress+Hauser to develop a tailored measurement concept. Together, the teams defined critical process parameters, identified key measurement points and selected technologies capable of providing reliable data under demanding operating conditions.

Promass Coriolis flowmeters enable high-accuracy measurement of gaseous CO₂, while additional instrumentation, including Prowirl vortex flowmeters for steam, Promag electromagnetic flowmeters for condensate flow and Liquicap for level measurement, provides visibility into key utility and process streams.

By combining these measurements, DACMA can correlate mass and energy balances across the entire process. This integrated data foundation supports process optimization, validates system performance and provides the transparency required to scale Direct Air Capture technology from pilot projects to industrial deployment.

联系我们

您对我们的产品组合感兴趣吗?想要谈谈您的实际应用吗?

请尽可能详细地告诉我们您的问题和需求,这样我们就能为您定制合适的解决方案了。

Products and services used

/

Related solutions and technology

温度测量

过程行业用温度计和变送器

更多信息

系统产品

系统和数据管理器产品概述 - 完整的解决方案

更多信息

软件解决方案

除了所有相关测量和系统技术,我们还提供适当的软件,用于各个分支行业,确保您的操作过程满负荷运行。

更多信息

压力测量 

适用于液体、气体和蒸汽的压力与差压测量

更多信息

Monitoring of effluent discharge 

Operate wastewater discharge within legal limits with complete, reliable monitoring for continuous values and fast response to contamination.

Read more

Hydrogen measurement in natural gas pipelines

Fast, continuous hydrogen measurement in natural gas pipelines enables safe blending, quality compliance and dynamic control using Raman spectroscopy - without consumables or flaring

Read more

Biomethane quality analysis for safe and compliant gas injection 

Ensure reliable biomethane quality with fast, accurate online measurement of H₂S, water dew point and critical parameters for safe grid injection and efficient operations. 

Read more

Protect reverse osmosis membranes with online water quality monitoring for desalination 

Reliable online water quality monitoring to protect RO (Reverse Osmosis) membranes, reduce cleaning effort, and extend membrane lifetime in desalination and water reuse applications

Read more

FAQs

企业商标 DACMA GmbH

DACMA GmbH总部位于汉堡,致力于研发和运营直接空气捕集(DAC)系统,用于从大气中去除CO₂。公司整合了机械、工艺及航空航天工程领域的专业技术,推出可靠且可规模化扩展的负排放技术。通过跨学科团队协作及包括巴西在内的国际项目,DACMA正推动DAC的工业化部署,并助力实现全球气候目标。